Feedback_Calibration_Current
Feedback_Calibration_Current
| Address: | 10282 (282AH) |
| Type: | UINT16 |
| Access: | Read/Write |
| Unit: | mA |
| Range: | 0 to (max drive current) |
| Default Value: | 1000 |
| Store Supported: | Yes |
| Description: | This value is used for Feedback feature and define current used during the calibration procedure. This value has to be enough to permit the motor to move in the point of maximum torque, in general it should be set to the maximum current that the motor can accept. |
| Notes: |
See Closed Loop Modality for details. |